AnsweredAssumed Answered

ADV7611 - Configuration

Question asked by crcn on Jun 23, 2015
Latest reply on Jun 23, 2015 by GuenterL

Hello,

I'm working in a project with ADV7611.

The project basically consist in:

 

HDMI receiver(ADV7611) -> H264 Encoder (FPGA) -> Modulator DVB (FPGA) -> Output

 

What I want is, regardless of the resolution that I have in the ADV7611input, passthrough to the H264 FPGA without changes.

 

My questions are:

1- For each resolution I have in input, I need to configure the ADV7611 (I see in the ADV7611-VER.3.0c.txt file there are several scripts for each resolution), or I can use only one? If yes, which one?

2- The EDID configuration in ADV7611-VER.3.0c.txt is working for my scenario, or I need to change that?

3- Each time I change of resolution, I need to configure the EDID?

 

The resolutions that I have in input are:

1920x1080 60p

1920x1080 50p

1920x1080 60i

1920x1080 50i

1920x1080 30p

1920x1080 25p

1280x720 60p

1280x720 50p

1280x720 30p

1280x720 25p

720x576 25i

704x480 30i

 

 

Thanks.

 

Regards,

Cesário

Outcomes