AnsweredAssumed Answered

zedboard alike platform + 9361+custom IP

Question asked by Nauman on Jun 23, 2015
Latest reply on Jul 6, 2015 by rejeesh

I have followed up the link for adding custom IP in the https://ez.analog.com/message/201329#201329 link.

I want to use No OS driver to make a flexible SDR which has baseband as an IP attached with the ARM on AXI or FIFO.

I have been able to synthesis the fmcomms2 design with all its IPs. 

 

The queries are following.

 

1: If i use FIFOs in front of my Baseband to pump I/Qs to the axi_9361 IP, than the software driver will stay the same? I will be able to access the configuration registers and control state of transceiver?

 

2: d2.jpg

what is the ADC_ADDRESS here? as if this is a normal FIFO than it will just have the width and depth not addresses. same as for the DAC FIFO.

 

3:

what are these addresses and where are they used?

 

http://wiki.analog.com/resources/fpga/docs/hdl/regmap

 

the over all picture i believe for my design using ad9361 fmcomms2 is as in this figure..

 

D1.jpg

please guide me in this..

 

Regards

Nauman

Outcomes