AnsweredAssumed Answered

ADV7619 to support 2800x2100 30Hz resolution

Question asked by JosephSh Employee on Jun 23, 2015
Latest reply on Jun 30, 2015 by JosephSh

Dear Sir,

     my customer Hikvison is using the ADV7619 on their large pannel and HD video conference system; it has already support the 4K*2K HDMI input sucessfully;  now their end customer need them to support the 2800x2100 30Hz HDMI/DVI input from PC, the detail time as attacehd picture:

  as the pixel clock is 187Mhz, it exceeds 170Mhz, customer uses the 48bit (2*24bit) output format, similar with the 4K*2K 30Hz setting; but the ADV7619 can not output right video signal (clock/HSYNC/VSYNC); by the ADV7619 STDI block, the resolution detection is right;

    below is the registers setting, please help to give your comments for this issue:

 

 

    /* :RGB  3840x2160 _@ 30 260MHz */

 

    {I2C_ADV7619_HDMI_MAP, 0xC0, 0x03}, //ADI Recommended Write

 

    {I2C_ADV7619_CP_MAP,   0xC9, 0x2C}, //Set DIS_AUTO_PARAM_BUFF 0

 

    {I2C_ADV7619_HDMI_MAP, 0x00, 0x08}, //Set HDMI Input Port A (BG_MEAS_PORT_SEL = 001b)

 

    {I2C_ADV7619_IO_MAP,   0x01, 0x26}, //Prim_Mode =110b HDMI-GR

 

    {I2C_ADV7619_IO_MAP,   0x02, 0xF2}, //Auto CSC, RGB out, Set op_656 bit

 

    {I2C_ADV7619_IO_MAP,   0x03, 0x54}, //2x24 bit SDR 444 interleaved mode 0

 

    {I2C_ADV7619_IO_MAP,   0x05, 0x28}, //AV Codes Off

 

    {I2C_ADV7619_IO_MAP,   0x06, 0xA0}, //inversion on VS,HS pins

 

    {I2C_ADV7619_IO_MAP,   0x0C, 0x42}, //Power up part

 

    {I2C_ADV7619_IO_MAP,   0x15, 0x80}, //Disable Tristate of Pins

 

    {I2C_ADV7619_IO_MAP,   0x19, 0x98}, //LLC DLL phase

 

    {I2C_ADV7619_IO_MAP,   0x33, 0x40}, //LLC DLL MUX enable

 

    {I2C_ADV7619_IO_MAP,   0xDD, 0xA0}, //LLC Half frequency

 

    {I2C_ADV7619_CP_MAP,   0xBA, 0x01}, //Set HDMI FreeRun

 

    {I2C_ADV7619_CP_MAP,   0xBF, 0x16}, //Set HDMI FreeRun output default colors as manual configuration

 

    {I2C_ADV7619_CP_MAP,   0xC0, 0x35}, //Set HDMI FreeRun colors G value

 

    {I2C_ADV7619_CP_MAP,   0xC1, 0x29}, //Set HDMI FreeRun colors R value

 

    {I2C_ADV7619_CP_MAP,   0xC2, 0xB2}, //Set HDMI FreeRun colors B value

 

    {I2C_ADV7619_KSV_MAP,  0x40, 0x83}, //BCAPS set to default

 

    {I2C_ADV7619_DPLL_MAP, 0xB5, 0x01}, //Setting MCLK to 256Fs

 

    {I2C_ADV7619_DPLL_MAP, 0xC3, 0x80}, //DI recommended writes (HiFreq)

 

    {I2C_ADV7619_DPLL_MAP, 0xCF, 0x03}, //DI recommended writes (HiFreq)

 

    {I2C_ADV7619_HDMI_MAP, 0x3E, 0x69}, //ADI reccommended writes

 

    {I2C_ADV7619_HDMI_MAP, 0x3F, 0x46}, //ADI reccommended writes

 

    {I2C_ADV7619_HDMI_MAP, 0x4E, 0x7E}, //ADI reccommended writes

 

    {I2C_ADV7619_HDMI_MAP, 0x4F, 0x42}, //ADI reccommended writes

 

    {I2C_ADV7619_HDMI_MAP, 0x02, 0x03}, //ALL BG Ports enabled           

 

    {I2C_ADV7619_HDMI_MAP, 0x57, 0xA3}, //ADI reccommended writes      

 

    {I2C_ADV7619_HDMI_MAP, 0x58, 0x07}, //ADI reccommended writes  

 

    {I2C_ADV7619_HDMI_MAP, 0x83, 0xFC}, //Enable clock terminators for port A & B

 

    {I2C_ADV7619_HDMI_MAP, 0x84, 0x03}, //FP MODE

 

    {I2C_ADV7619_HDMI_MAP, 0x85, 0x10}, //ADI recommended setting

 

    {I2C_ADV7619_HDMI_MAP, 0x86, 0x9B}, //ADI recommended setting

 

    {I2C_ADV7619_HDMI_MAP, 0x89, 0x03}, //HF Gain

 

    {I2C_ADV7619_HDMI_MAP, 0x9B, 0x03}, //ADI recommended setting

 

 

 

 

 

 

Outcomes