AnsweredAssumed Answered

AD-FMCOMMS1-EBZ REV B testing problems based on Xilinx_kc705

Question asked by woxunzhaoziwo on Jun 22, 2015
Latest reply on Jun 29, 2015 by AdrianC

Our testing of AD-FMCOMMS1-EBZ REV B is not successful, two errors:

1.After the hardware is generated on Vivado2014.2, the "elf" file based on software projects from the reference

   link can't  be downloaded successfully. The SDK says"target is not responding(timed out) "

   (reference link::ADI Reference Designs HDL User Guide [Analog Devices Wiki])

2.Sometimes the elf file can be downloaded, but the program stops at

                    /* Wait until the current transfer is completed. */

                      do {

                          reg_val = Xil_In32(baddr + AXI_DMAC_REG_IRQ_PENDING);

                         }

                       while(reg_val != (AXI_DMAC_IRQ_SOT | AXI_DMAC_IRQ_EOT));

   (reference link :: AD-FMCOMMS1-EBZ Quick Start Guide on Xilinx FPGA Boards Without OS [Analog Devices Wiki])

   (software version:: no-OS-2014_R2)



thanks very much!!!!

 

Outcomes