AnsweredAssumed Answered

MPEG-4 SP/ASP Encoder API Problem

Question asked by deepak on Apr 5, 2011
Latest reply on Apr 20, 2011 by RatheeshMallaya

Hello All,

I am trying to use MPEG-4 SP/ASP Encoder for a wireless application. My target plateform is BF561 and I am using EZKit Lite board (rev 2.3)for the same. I want to read the compressed bit stream stored in SDRAM and transmit it through SPORT. I am usingPAL resolution and taking data in real time through PPI. How could i get the actual start and end addresses  of the SDRAM where compressed bit stream is written. I have also seen the .ldf file to get start and end addresses for the bitstream. But end address of the bitstream buffer A in SDRAM is not looking fixed and also with PAL resolution bit stream buffer B is not updating at all. It seems that for PAL resolution, the bit stream is written only in bitstream buffer A. So can anybody please suggest me how to get the actual start and end addresses of the compressed stream in SDRAM.

Thanks & Regards

Deepak

Outcomes