AnsweredAssumed Answered

ADN4695E bus termination in a point-to-point topology

Question asked by luiz.mellucci on Jun 19, 2015
Latest reply on Jun 22, 2015 by RAnslow

We're using ADN4695E in a point-to-point topology with a 100Ω termination at line end.

 

ADN4695E datasheet says "Supported bus loads: 30 Ω to 55 Ω".

 

But we're not sure if it's for a multi-point bus, as AD4695E is suitable for, or if it applies also for point-to-point topology.

 

Is there any problem in using a 100Ω termination with ADN4695E as transceivers of a point-to-point bus?

 

Thanks.

Outcomes