AnsweredAssumed Answered

Update to 2014_R2-2015_04_24.img.xz result no HDMI output

Question asked by fivepanda on Jun 18, 2015
Latest reply on Jun 23, 2015 by fivepanda

Hello everybody!

I have problem on building new 2014_R2-2015_04_24 image to zc706 board(with fmcomms6 card), and now I want someone can geive some help!

The problem discription:

1.     I followed the guide Zynq & Altera SoC Quick Start Guide [Analog Devices Wiki] , downloaded the 2014_R2-2015_04_24 image files,

        I have a 8GB SD card, then I followed the script Linux Download and setting up the image [Analog Devices Wiki] , on my             

        pc(ubuntu), the SD card mount as /dev/sdb, so I changed /dev/mmcblk0 to /dev/sdb, is that right?

 

2.     After step1, I have img copied to SD card, compared to earlier img , the linaro rootfs seems missed a selinuxfs file, is it correct?

       I copied the fmcomms6 bootrom to fat32 partition, now I had all things get ready!

 

3.     Plug the SD card into the board, then I launch the board, linux boots up, from the serail I can see linux command line works well.

        But HDMI has no output, the boot command output is as follows:

    


------------------------------------------------------------------------------------------------------------------------------------------

380 bytes read in 9 ms (41 KiB/s)

Loaded environment from uEnv.txt

Importing environment from SD ...

Running uenvcmd ...

Copying Linux from SD to RAM...

reading uImage

3427856 bytes read in 313 ms (10.4 MiB/s)

reading devicetree.dtb

13394 bytes read in 30 ms (435.5 KiB/s)

reading uramdisk.image.gz

** Unable to read file uramdisk.image.gz **

## Booting kernel from Legacy Image at 03000000 ...

   Image Name:   Linux-3.19.0

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3427792 Bytes = 3.3 MiB

   Load Address: 00008000

   Entry Point:  00008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 02a00000

   Booting using the fdt blob at 0x2a00000

   Loading Kernel Image ... OK

   Loading Device Tree to 1fff9000, end 1ffff451 ... OK

 

 

Starting kernel ...

 

 

Uncompressing Linux... done, booting the kernel.

Booting Linux on physical CPU 0x0

Linux version 3.19.0 (root@ubuntu) (gcc version 4.6.3 (Sourcery CodeBench Lite 2012.03-79) ) #1 SMP PREEMPT Wed Jun 17 09:47:47 CST 2015

CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: Xilinx Zynq ZC706

bootconsole [earlycon0] enabled

cma: Reserved 128 MiB at 0x38000000

Memory policy: Data cache writealloc

PERCPU: Embedded 9 pages/cpu @eefd5000 s7552 r8192 d21120 u36864

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260624

Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 901604K/1048576K available (4385K kernel code, 265K rwdata, 1716K rodata, 208K init, 132K bss, 15900K reserved, 131072K cma-reserved, 139264K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

    vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)

    lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .text : 0xc0008000 - 0xc05fd798   (6102 kB)

      .init : 0xc05fe000 - 0xc0632000   ( 208 kB)

      .data : 0xc0632000 - 0xc06747c0   ( 266 kB)

       .bss : 0xc06747c0 - 0xc06958ac   ( 133 kB)

Preemptible hierarchical RCU implementation.

        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.

RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2

NR_IRQS:16 nr_irqs:16 16

L2C: platform modifies aux control register: 0x72360000 -> 0x72760000

L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000

L2C-310 erratum 769419 enabled

L2C-310 enabling early BRESP for Cortex-A9

L2C-310 full line of zeros enabled for Cortex-A9

L2C-310 ID prefetch enabled, offset 1 lines

L2C-310 dynamic clock gating enabled, standby mode enabled

L2C-310 cache controller enabled, 8 ways, 512 kB

L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001

slcr mapped to f0006000

zynq_clock_init: clkc starts at f0006100

Zynq clock init

sched_clock: 16 bits at 54kHz, resolution 18432ns, wraps every 1207951633ns

timer #0 at f0008000, irq=16

Console: colour dummy device 80x30

Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)

Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x422d48 - 0x422da0

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

Brought up 2 CPUs

SMP: Total of 2 processors activated (2664.03 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

zynq-ocm f800c000.ps7-ocm: ZYNQ OCM pool: 256 KiB @ 0xf0080000

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

media: Linux media interface: v0.10

Linux video capture interface: v2.00

EDAC MC: Ver: 3.0.0

Advanced Linux Sound Architecture Driver Initialized.

Switched to clocksource ttc_clocksource

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 3, 32768 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available

futex hash table entries: 512 (order: 3, 32768 bytes)

bounce: pool size: 64 pages

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

dma-pl330 f8003000.ps7-dma: Loaded driver for PL330 DMAC-241330

dma-pl330 f8003000.ps7-dma:     DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16

e0001000.uart: ttyPS0 at MMIO 0xe0001000 (irq = 20, base_baud = 3125000) is a xuartps

郼onsole [ttyPS0] enabled

console [ttyPS0] enabled

bootconsole [earlycon0] disabled

bootconsole [earlycon0] disabled

xdevcfg f8007000.devcfg: ioremap 0xf8007000 to f0072000

[drm] Initialized drm 1.1.0 20060810

drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_drv.c:axi_hdmi_platform_probe[176]

platform 70e00000.axi_hdmi: Driver axi-hdmi requests probe deferral

brd: module loaded

loop: module loaded

m25p80 spi32765.0: found s25fl128s, expected n25q128a11

m25p80 spi32765.0: s25fl128s (32768 Kbytes)

5 ofpart partitions found on MTD device spi32765.0

Creating 5 MTD partitions on "spi32765.0":

0x000000000000-0x000000500000 : "boot"

0x000000500000-0x000000520000 : "bootenv"

0x000000520000-0x000000540000 : "config"

0x000000540000-0x000000fc0000 : "image"

0x000000fc0000-0x000002000000 : "spare"

libphy: XEMACPS mii bus: probed

xemacps e000b000.eth: pdev->id -1, baseaddr 0xe000b000, irq 33

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver usbserial_generic

usbserial: USB Serial support registered for generic

usbcore: registered new interface driver ftdi_sio

usbserial: USB Serial support registered for FTDI USB Serial Device

e0002000.usb supply vbus not found, using dummy regulator

ULPI transceiver vendor/product ID 0x0424/0x0007

Found SMSC USB3320 ULPI transceiver.

ULPI integrity check: passed.

ci_hdrc ci_hdrc.0: EHCI Host Controller

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

i2c /dev entries driver

i2c i2c-0: Added multiplexed i2c bus 1

i2c i2c-0: Added multiplexed i2c bus 2

at24 3-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write

i2c i2c-0: Added multiplexed i2c bus 3

pca953x 4-0021: interrupt support not compiled in

i2c i2c-0: Added multiplexed i2c bus 4

rtc-pcf8563 5-0051: chip found, driver version 0.4.3

rtc-pcf8563 5-0051: rtc core: registered rtc-pcf8563 as rtc0

i2c i2c-0: Added multiplexed i2c bus 5

i2c i2c-0: Added multiplexed i2c bus 6

at24 7-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write

i2c i2c-0: Added multiplexed i2c bus 7

i2c i2c-0: Added multiplexed i2c bus 8

pca954x 0-0074: registered 8 multiplexed busses for I2C switch pca9548

zynq-edac f8006000.ps7-ddrc: ecc not enabled

Xilinx Zynq CpuIdle Driver started

Driver 'mmcblk' needs updating - please use bus_type methods

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

sdhci-arasan e0100000.sdhci: No vmmc regulator found

sdhci-arasan e0100000.sdhci: No vqmmc regulator found

mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA

ledtrig-cpu: registered to indicate activity on CPUs

hidraw: raw HID events driver (C) Jiri Kosina

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

si570 1-005d: registered, current frequency 156250000 Hz

platform 79020000.axi-ad9652-lpc: Driver cf_axi_adc requests probe deferral

spi spi32766.1: Driver ad9467 requests probe deferral

mmc0: new high speed SDHC card at address 0002

mmcblk0: mmc0:0002 00000 7.41 GiB

mmcblk0: p1 p2 p3

ad9517 spi32766.0: probed

spi32766.2 supply vcc not found, using dummy regulator

adv7511-hdmi-snd fpga-axi@0:adv7511_hdmi_snd: adv7511 <-> 75c00000.axi-spdif-tx mapping ok

TCP: cubic registered

NET: Registered protocol family 17

Registering SWP/SWPB emulation handler

usb 1-1: new low-speed USB device number 2 using ci_hdrc

Console: switching to colour frame buffer device 170x48

axi-hdmi 70e00000.axi_hdmi: fb0:  frame buffer device

axi-hdmi 70e00000.axi_hdmi: registered panic notifier

[drm] Initialized axi_hdmi_drm 1.0.0 20120930 on minor 0

platform 79020000.axi-ad9652-lpc: Driver cf_axi_adc requests probe deferral

input: Generic USB K/B as /devices/soc0/amba@0/e0002000.usb/ci_hdrc.0/usb1/1-1/1-1:1.0/0003:13BA:0017.0001/input/input0

oooooooo|ooooooo-----------------

  DCO 0x7 CLK 250000000 Hz

cf_axi_adc 79020000.axi-ad9652-lpc: ADI AIM (8.00.b) at 0x79020000 mapped to 0xf05e0000, probed ADC AD9652 as MASTER

input: gpio_keys as /devices/soc0/gpio_keys/input/input1

hid-generic 0003:13BA:0017.0001: input,hidraw0: USB HID v1.10 Keyboard [Generic USB K/B] on usb-ci_hdrc.0-1/input0

rtc-pcf8563 5-0051: setting system clock to 1970-02-04 17:31:35 UTC (3000695)

input: Generic USB K/B as /devices/soc0/amba@0/e0002000.usb/ci_hdrc.0/usb1/1-1/1-1:1.1/0003:13BA:0017.0002/input/input2

ALSA device list:

  #0: HDMI monitor

hid-generic 0003:13BA:0017.0002: input,hidraw1: USB HID v1.10 Mouse [Generic USB K/B] on usb-ci_hdrc.0-1/input1

EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

VFS: Mounted root (ext4 filesystem) on device 179:2.

devtmpfs: mounted

Freeing unused kernel memory: 208K (c05fe000 - c0632000)

Mount failed for selinuxfs on /sys/fs/selinux:  No such file or directory

* Setting up X socket directories...       tropy available              [ OK ]

* Starting IIO Daemon iiod                                              [ OK ]

 

 

Last login: Wed Feb  4 17:27:44 UTC 1970 on tty1

Welcome to Linaro 14.04 (GNU/Linux 3.19.0 armv7l)

 

 

* Documentation:  https://wiki.analog.org/ https://ez.analog.com/

 

 

  -------------------------------------------------------------------------------------------------------------------------------------------

------------------------------------------------------------------------------------------------------------------------------------------

 

     Then I manually input "startx":

 

xauth:  file /root/.Xauthority does not exist

 

 

 

 

X.Org X Server 1.15.1

Release Date: 2014-04-13

X Protocol Version 11, Revision 0

Build Operating System: Linux 3.2.0-58-highbank armv7l Ubuntu

Current Operating System: Linux analog 3.19.0 #1 SMP PREEMPT Wed Jun 17 09:47:47 CST 2015 armv7l

Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait

Build Date: 16 April 2014  01:41:53PM

xorg-server 2:1.15.1-0ubuntu2 (For technical support please see http://www.ubuntu.com/support)

Current version of pixman: 0.30.2

        Before reporting problems, check http://wiki.x.org

        to make sure that you have the latest version.

Markers: (--) probed, (**) from config file, (==) default setting,

        (++) from command line, (!!) notice, (II) informational,

        (WW) warning, (EE) error, (NI) not implemented, (??) unknown.

(==) Log file: "/var/log/Xorg.1.log", Time: Wed Feb  4 17:32:02 1970

(==) Using system config directory "/usr/share/X11/xorg.conf.d"

setversion 1.4 failed: Permission denied

Initializing built-in extension Generic Event Extension

Initializing built-in extension SHAPE

Initializing built-in extension MIT-SHM

Initializing built-in extension XInputExtension

Initializing built-in extension XTEST

Initializing built-in extension BIG-REQUESTS

Initializing built-in extension SYNC

Initializing built-in extension XKEYBOARD

Initializing built-in extension XC-MISC

Initializing built-in extension SECURITY

Initializing built-in extension XINERAMA

Initializing built-in extension XFIXES

Initializing built-in extension RENDER

Initializing built-in extension RANDR

Initializing built-in extension COMPOSITE

Initializing built-in extension DAMAGE

Initializing built-in extension MIT-SCREEN-SAVER

Initializing built-in extension DOUBLE-BUFFER

Initializing built-in extension RECORD

Initializing built-in extension DPMS

Initializing built-in extension Present

Initializing built-in extension DRI3

Initializing built-in extension X-Resource

Initializing built-in extension XVideo

Initializing built-in extension XVideo-MotionCompensation

Initializing built-in extension SELinux

Initializing built-in extension XFree86-VidModeExtension

Initializing built-in extension XFree86-DGA

Initializing built-in extension XFree86-DRI

Initializing built-in extension DRI2

Loading extension GLX

setversion 1.4 failed: Permission denied

shuto^Hd^H^Hddd^Cxinit: connection to X server lost

 

 


------------------------------------------------------------------------------------------------------------------------------------------

------------------------------------------------------------------------------------------------------------------------------------------


Before post this question , I googled and search on the EZONE, unfortunately find no exact answers...

Anyone can give help?@

Outcomes