AnsweredAssumed Answered

Loader file *.ldr for ADSP-21060

Question asked by manju.prabhakar on Jun 18, 2015
Latest reply on Dec 31, 2015 by Kader.M

Hi,

The ldr file generated using VisualDSP 5.0 version is different when generated from VisualDSP version 4.5. After comparing the two ldr files, I found that the Boot Kernel + 2 lines is the same in boot image which is similar to the example given in EE-56. But for the old working version, the user code starts as

:20062A000E0000000000090000010200000000F003000000001000000000000000006568C6

but new version starts as

:0C062A00020000000000050000000300BA

 

The old version runs well when flashed into the board. The new version runs only through emulation, but it runs with errors when booted from flash.

 

Please let me know why the user code start up is different, if you have faced similar issues please help.

 

Regards

Manju

Outcomes