AnsweredAssumed Answered

ADG712 specification

Question asked by tneagoe on Jun 17, 2015
Latest reply on Jun 18, 2015 by Stephen_Nugent

Hello there,

 

I want to use the ADG712BRUZ  @ 40 mA  3.3v 70C with 5 ms pulse.

 

Presently we are using the the ADG1612, same conditions.

The problem is that in the ADG1612 specification, rev b, page 7 table 5,

we can see that at 125C,  Vdd=3.3v, Imax = 70mA?!?

 

This table is not available for the ADG712BRUZ?!? What can we assume?

 

Question: CAN WE USE THE ADG712 AT 40 mA ( if a single channel is used)?

 

PLease advise,

Teodor

Outcomes