AnsweredAssumed Answered

No-OS design on a SD card

Question asked by jeffkt2 on Jun 17, 2015
Latest reply on Jun 18, 2015 by DragosB

Hi,

 

I'm trying to boot the FMCOMMS1 No-OS reference design from a SD card on a Zedboard. I've verified the application runs just fine if I execute through a SDK run configuration. I've then created a BOOT.BIN image by using the bootimage tool in SDK. I've arrange the following files on there:

 

1. fmcomms1 fsbl application (.elf)

2. zed hdl design (.bit)

3. fmcomms1 application (.elf)

 

The application successfully boots, but I see the following message on the serial port:

 

Running XCOMM Test Program

 

Initializing XCOMM I2C...

XCOMM Init I2C Failed!

 

Is there another setting that I'm missing?

 

Thanks for any help!

Outcomes