AnsweredAssumed Answered

ADV7619 free-run mode & output format

Question asked by @Jake@ on Jun 17, 2015
Latest reply on Jun 19, 2015 by mattp

Some questions. When used ADV7619...

I hope to please make sure that following conditions.

 

 

1. I would like to receive video. Resolution is as follows : 640x480p30 ~ 4K(4096x2160p24)

Is it possible?

 

2. If I am receiving the video below 1080p60.

Exactly, 640x480p30 ~ 1920x1080p60.

Operation mode is free-run mode. The output format is like to use the 24bit 422 format,

and want to use HS, VS, and FIELD output signals.

 

Thanks for you support.

Outcomes