AnsweredAssumed Answered

Memory browser(L2 Area) not working in CCES

Question asked by Mack on Jun 17, 2015
Latest reply on Sep 28, 2015 by Kader.M

Hello,

 

I loaded data into L2 memory area. Then I checked data loaded via Image viewer and it was good.

However I encountered a problem when I checked the same area via memory browser.

From the same L2 area of memory browser, only garbage data were observed.

Is it a bug of CCES?

My target is BF609 ezkit. CCES version is 1.2.0.

Memory browser.PNG

 

Below is my code.

 

volatile unsigned short* ptr = (unsigned short*)0xC8090000;

void main(void)
{
int i;

adi_initComponents();

CGU_Init(20,1,2); // CCLK:500MHz, SYSCLE/DDR:250MHz, SCLK1/SCLK2: 125MHz

    ConfigSoftSwitches_BF609();

    for(i=0;i<160*120;i++)
    {
     *ptr++ = 0x1080;
    }

while(1);
}

 

Best Regards,

Mack

Attachments

Outcomes