AnsweredAssumed Answered

Half-duplex SPORT on BF561

Question asked by Laz on Mar 29, 2011
Latest reply on Mar 30, 2011 by Laz

I need to connect a SHARC 21368 to a Blackfin 561.  I have existing code for the '368 which runs in half-duplex mode very well.  I'm planning to connect the BF561 in the same way by shorting the TX and RX port pins together (CLK-CLK, Frame-Frame, etc).  Anyone see a problem with this?  I haven't yet written the BF561 SPORT drivers to handle this, but I think it should work.

 

TIA.

Dan

Outcomes