AnsweredAssumed Answered

OP284

Question asked by op1ck on Jun 15, 2015
Latest reply on Jun 16, 2015 by JinoL

Hello engineers,

 

I want to design differential amplifier using OP284. They are consisted of 8 pins. Pin 2 and 3 are used for input signal A, + and -. Pin 5 and 6 are used for input signal B, + and -. With this component OP284 I need to read data from rotor sensor which are consisted 5 pins. Two of them are output signal pins. My question is, how to connect all pins 2,3,5 and 6 to rotor censor which are having only 2 output signal pins.

 

In attachment you can see my rotor censor.

 

Your sincerly

Attachments

Outcomes