AnsweredAssumed Answered

Looking for differential buffer

Question asked by Toshi on Jun 15, 2015
Latest reply on Jun 26, 2015 by iamPhil

Hi,

 

I'm looking for a differential buffer having following specs for 3m board to board connection. Can I have your advice?

 

  • Data rate: 1.6 to 1.8Gbps
  • Differential swing: 400mV ( max ) meaning single-end swing is 800mV ( max )
  • Output offset voltage: 1.2V ( typ ), 2.0V ( max ) - programmability preferred

 

Regards,

Toshi

Outcomes