AnsweredAssumed Answered

AD9228, single-end configuration

Question asked by sin on Jun 15, 2015
Latest reply on Jun 22, 2015 by DougI

I have some questions about AD9228.

 

   In fig.50 of the datasheet, single-end input configuration, the source voltage is
   displayed as 2Vp-p.  If the source voltage is 2Vp-p, the input voltage of AD9228 is
   0.9V +/-1V (i.e. -0.1V to 1.9V).    Is -0.1V input voltage available in AD9228 ?

   If not, will you share your understanding ?
   I am wondering that the actual input voltage of AD9228 is 1Vp-p.
   Please find attuched files. Is my understandingcorrect ?

 

Best Regards,

Attachments

Outcomes