AnsweredAssumed Answered

file export memory refresh

Question asked by genp on Mar 28, 2011
Latest reply on Mar 29, 2011 by BrettG

please, urgently need memory refreshing on the file export.

I worked with the ADU1446 last year, succesfully exported files and implemented them in a microcontroller project.

In the _IC_1.h of the last year project I see the parameter RAM definitions and array:

 

#define PARAM_SIZE 564
#define PARAM_ADDR 0
ADI_REG_TYPE Param_Data[PARAM_SIZE] = {
......};

 

Also it was a function in the default_download() of this file:

SIGMA_WRITE_REGISTER_BLOCK( DEVICE_ADDR_IC_1, PARAM_ADDR, PARAM_SIZE, Param_Data );

 

When I export files now, I don't see the parameter RAM definitions and array (and can't find them anywhere).

Also, instead of the above function there is:

SIGMA_WRITE_REGISTER_BLOCK( DEVICE_ADDR_IC_1, _ADDR, _SIZE, _Data );

 

and compiler complains that _ADDR, _SIZE and _Data are not defined.

 

Even more, when I export the files for the last year project with the version of SigmaStudio I used that time,

I get the same results as now.

 

What am I missing ?

Outcomes