AnsweredAssumed Answered

ZC706-FMCOMMS1-AD9548 Configuration via Linux

Question asked by Zc706-user on Jun 13, 2015
Latest reply on Jun 25, 2015 by Zc706-user

HI all,

 

I'd like to move the input reference frequency into the ad9548 on the FMCOMMS1 board from 30.72 MHz to 32.5 MHz. I presume the configuration is done as part of the Linux driver initialization. I've modified the ZC706 to output the 32.5 MHz reference; I just need some help with a procedure to modify the ad9548 configuration parameter.

 

THanks

Outcomes