vinodbableshwar

ADSP-SC58x/2158x SPI - Example Code

Discussion created by vinodbableshwar on Jun 12, 2015

The attached code is used for data transfer using SPI peripheral. Any of the SPI instances can be used as master or slave with each SPI being a Tx or Rx. There are macros to select between the various configuration options. The same code can used for core mode or DMA mode data transfer.

Outcomes