AnsweredAssumed Answered

ADSP-SC58x/2158x TMU: Example code

Question asked by Nabeel Employee on Jun 12, 2015

Attached code demonstrates a simple example in which the code reads the temperature from TMU at regular intervals and displays the measured temperature on console in floating point format. Code provides to options to configure following setting in the TMU:

  1. Enable/Disable Averaging
  2. Configure Gain and offset setting
  3. Configure Alert and Fault thresholds

 

Codes are provided for both ARM and SHARC cores

Attachments

Outcomes