AnsweredAssumed Answered

Evaluation Board UG-209 firmware source code?

Question asked by gundamned on Mar 25, 2011
Latest reply on Mar 25, 2011 by CraigG

Hello,

 

recently I bought the UG-209 evaluation board, and I am wondering if anyone could provide me the source code of the firmware.hex file bundled in the CD of the evaluation board. It is the firmware running on the MCU. It would be really helpful to understand the programming tecniques used for:

1) data communication protocol betweeen the MCU (an ADuC7026) and the accelerometer (an ADXL312);

2) how to sample data efficiently at high frequencies (3200Hz) on the accelerometer;

3) filtering and anti-aliases techniques used in the eval board.

 

The eval board provides also a good application PC side which uses the LabView runtime, it would be really useful to have the source code for that application too.

 

TIA

Mark

Outcomes