AnsweredAssumed Answered

ADV7623 1080P60 1080P50 cann't output

Question asked by Hayden on Jun 9, 2015
Latest reply on Jun 11, 2015 by Hayden

Now Adv7623 can support 480P 576P 480i 576i 720P 1080i 1080P24 1080p30,but it cann't support 1080P60 1080P50.

When the input of adv7623 is 1080P60, the output TMDS CLOCK is 148.5MHz when I used oscilloscope to detect it,and the TX Main Map reg0x3D is 0x10,but the monitor cann't detect the video signal that it's output from adv7623.

If there is no signal input to the adv7623,the monitor can display the1080 OSD which it's generated by Adv7623.

 

What should I configure when input 1080P60 or108050?

 

Attached is my configuration !

Outcomes