AnsweredAssumed Answered

ADG701/702 710L/702L as low current road switch

Question asked by ricky on Jun 8, 2015
Latest reply on Jun 14, 2015 by ricky

Hi All,

 

One of my customer wants low Iq road switch.

The Iq of ADP198 is 2.5uA typ/ 20uA max and is too large for his application.

The road current for his application is 10mA or less.

His supply voltage is 5.5V.

Then I will propose ADG701/702 or ADG701L/702L instead of ADP198.

I would like to double check with you that ADG701/702, ADG701L/702L can be used as low road current road switch.

Is there any precautions needed in this application?

 

Best Regards,

Ricky

Outcomes