AnsweredAssumed Answered

AD9361 - RX LO and TX LO Freq. band? Freq Band in baseband?

Question asked by rzubillaga on Jun 8, 2015
Latest reply on Jun 12, 2015 by tlili

Hi all,

 

Regarding AD9361 datasheet (RF Agile Transceiver), its frequency band is from 70 MHz to 6 GHz. This frequency band is supposed to be the RF frequency band.

I would like to know which the RX LO and TX LO frequency band are. I supposed that the frequency band of both of them (RX LO and TX LO) is the same, and is it form 47 MHz to 6 GHz? According the to Reference Manual, I think so but I would like to confirm it…

Beside I would like to know which is the frequency band in baseband after downconverting signals… in Rx signal path (I suppose that it is the same in the Tx signal path).

 

On the other hand, I wonder if the parallel data ports (P0 and P1) can  operate independently to transfer data between each transceiver (of this device) and the baseband processor.

 

Thank you for your help!

Outcomes