AnsweredAssumed Answered

Can I connect +12V power supply to ADP5071 EVB and get +/-5V output?

Question asked by plkmn3 on Jun 7, 2015
Latest reply on Jun 9, 2015 by Jason_Duan

Hi;

 

We have a application which need convert +12V input to +/-5V outputs with +/-1A loads. I saw the ADP5071 is just suitable for this. Now I want to buy a EVB to try, but I checked the datasheet of the EVB, it said the input range is 3 V to 5.5 V. Can I modify some components on the board and get +12V input and +/-5V output?

 

THX!

 

Donald

Outcomes