AnsweredAssumed Answered

IF Receiver for 3 to 400MHz

Question asked by ErichNast on Jun 5, 2015
Latest reply on Jun 22, 2015 by bsam

I am looking to design an IF receiver with input freq range from 3 to 400MHz and struggling to find a suitable Mixer with integrated LO.

I came across the ADRF6655 which is the right type of part, except for the input freq range;

  • RF input frequency range: 100 MHz to 2500 MHz

Are there any similar products from ADI or alternate ideas I can consider for my freq range.

I want to use a baseband freq of 1Mhz which I will feed into an AD7760 ADC.

 

Thanks

Erich Nast

Outcomes