AnsweredAssumed Answered

AD8065 SPICE model's noise performance is incorrect

Question asked by zhaoming on Jun 4, 2015
Latest reply on Jun 5, 2015 by zhaoming

I use the SPICE model downloaded from the ADI website of AD8065 and configured as a G=+1 buffer and simulate for the ouput nosie density. It is supposed to be the same with the  equivalent input noise density. But the part of 1/f noise is missing and the white noise is much lower than that in datasheet, the noise above 10MHz is too large compared with the value in datasheet. Is the SPICE model of AD8065 so inaccurate on noise performance?  The model of AD8033 also has the same kind of problem.

Outcomes