AnsweredAssumed Answered

ADV7180 linux v4I2 api

Question asked by pjxan Employee on Jun 3, 2015
Latest reply on Jun 4, 2015 by DaveD

Hi !

 

I've a customer that are working with the ADV7180 in one of their applications :

 

"We are using ADV7180.c to configure the ADV7180 chip. On top of it we are using standard v4l2 api. What we see is that the image quality is not perfect. We have compared a competitor part and an AD7180 evalboard from Analog Devices . And there are no real differences in the quality so it can be ignored . But it would be interesting to see if this can be optimized in SW.

 

Also , we see sync problems. If you lose power to the camera and it comes back the picture rolls a few laps. Perhaps this can be resolved/improved with an optimized driver as well."

 

Is there any improved drivers for the EDV7180 ?

 

BR Patrik

Outcomes