AnsweredAssumed Answered

ADA4700-1 with large capacitive load

Question asked by tomi on May 27, 2015
Latest reply on May 28, 2015 by tomi

One of potential applications of ADA4700-1 is a piezo driver, but solutions presented in the datasheet work up to 100nF only, while my piezo has 1.5uF. Could you suggest a circuit which would work fine in such a case? I need to work with the frequencies from DC up to 35 kHz

Outcomes