AnsweredAssumed Answered

HMC997 and HMC565 Demo-board Capacitors

Question asked by hmgps on May 26, 2015
Latest reply on May 29, 2015 by kkaya

Hello,

 

I am experiencing some differences between my PCB's (replicas of the demo boards) using these integrated circuits and the demo board that I ordered from Hittite. As these differences are the same and occur on the same bands (approx 17 GHz) in both HMC997 and HMC565, I am concluding that my experience is due to different capacitors.

 

I would like to know, if possible, what are the manufacturers and models of the 100 pF RF choke capacitors used in both these demo boards.


P.S.: The transmission lines impedances (in CPW) were validated using HFSS. They were adjusted to be 50 Ohm.

 

Thanks in advance,

 

Hugo Santos

Outcomes