AnsweredAssumed Answered

ADP3339 minimum input power and tolerance

Question asked by PeterPWL on May 22, 2015
Latest reply on Jun 16, 2015 by jespirit

According to the datasheet ADP3339 has a 2.8 V to 6 V input voltage range. We currently use this device in our design which feed in only 2.48V at the input due to design limitation. I understand that this is not ideal but so far we have minimal fall-out. Without specifying in a new part, could someone please explain the impact of providing insufficient input power and the risk/failure symptoms?

 

Thanks.

Peter

Outcomes