AnsweredAssumed Answered

ADF4159 and ADF4155 Cycle Slip Reduction Differences

Question asked by Ivan-Rusov Employee on May 22, 2015
Latest reply on May 25, 2015 by Ivan-Rusov

Hi,

 

ADF4159 contains following sentence in the datasheet (page #17): "The cycle slip reduction feature can be used only when the phase detector polarity setting is positive (Bit DB6 = 1 in Register R3). CSR cannot be used if the phase detector polarity setting is negative (Bit DB6 = 0 in Register R3)."

 

While ADF4155 does not have the sentence.

 

Could ADF4155 Cycle Slip Reduction feature be used if the phase detector polarity setting is either negative or positive?

 

Regards,

Ivan

Outcomes