AnsweredAssumed Answered

AD6645-80 Error in ADC Codes

Question asked by Philipp123 on May 22, 2015
Latest reply on May 22, 2015 by Philipp123

Hi,

we have designed a digitizer board with 3 ADCs. Two of them are pin compatible adcs from another vendor and one is the AD6645ASVZ-80. We have some problems with this AD data converter!

 

1. Example: Sampling Frequency 40MHz, Input Sine 10k

40MSPS_10kSine_error.png

The source of this bit toggling is the AD6645. I can measure this also with an analog scope. The fpga works correct.

error_cut.png

2. I observed different patterns of error codes. It depends on the sampling frequency. Here's another example

Sampling Freq: 80MSPS, 1k Sine

80MSPS_1kSine.png

 

I think this IC is defective. What should i do?

 

Best regards,

Philipp

Outcomes