AnsweredAssumed Answered

reset 9361 to default config

Question asked by rrogers on May 21, 2015
Latest reply on May 21, 2015 by rrogers

Hi, is there an easy way to reset the fmcomms (9361) to the power up default configuration from the device tree?  The use case is having multiple applications, not running at the same time, that perform some rx/tx operations.  When one application starts up, it would be easier to do a simple reset to have the 9361 in a known state, instead of trying to figure out the current state, as left by the previous application.

 

Outcomes