AnsweredAssumed Answered

A/D D/A Multiple ground considerations

Question asked by davegold on May 19, 2015
Latest reply on May 20, 2015 by BrenS

Hello all,

 

I am designing a PCB with 3 AD7853 A/Ds and 1 AD5323 D/A.

The board has a ground layer with separate analog and digital ground planes.

It also has to power layers.

I have the following questions. They get trickier as you go.

 

1) I understand from reading tech notes that GND pin 15 of the AD5323 D/A

    should be connected to the analog ground plane. Is that correct?

 

2) It appears that GND pin 19 of the AD7853 A/D should be connected to the

    analog ground plane as well as the AGND pins 6 & 12?

 

3) Should the other AD7853 A/D pins that are connected to resistors to ground

    like POLARITY (14), SM1 (15), SM2 (16) also go to analog ground, rather than

    the digital ground?

 

4) Should the DVDD bypass capacitor go to analog ground or digital ground?

    I wonder because of 2).

 

5) Since I have four mixed digital/analog chips, how should I tie the analog ground

    plane to the digital ground plane.  I read in one tech note that I should tie the planes

   together under each of the chips.  Another place suggested I ties them in one place

   with a 3.9 ohm resistor.

 

6) I have some space on my power planes where I could have additional analog ground planes

   parallel to the one on the ground plane.  Is this better? Worse (maybe create ground loops?)

 

Thanks!

 

+++ Dave

Outcomes