AnsweredAssumed Answered

Memory of CED1z

Question asked by Marcel on May 19, 2015
Latest reply on May 21, 2015 by KarenNE

Good Morning,

 

I am using EVAL-ADAS3022EDZ working with converter evaluation and development CED1Z and using USB Blaster.

I would like to configure the memory address on CED1z which has two 2MB SRAM memories.

It is possible to access by Quartus II? And it is possible one by one? Or they are treated just as one module? Could be possible to obtain a memory map of these memories?

 

I would also like to execute my aplication through Matlab. Could you provide some information about that?

Thank you very much in advance.

 

Further information:

I connect the USB Blaster from PC to JTAG input in CED1Z where I can control the FPGA and program the image (ced1z.sof) using NIOS II (ADIEvalBoard.elf).

I also control the FPGA located in EVAL-ADAS3022 where I programmed with .pof file in order to capture a data adquisition. (Just like is explained in this link: https://www.google.es/url?sa=t&rct=j&q=&esrc=s&source=web&cd=2&cad=rja&uact=8&ved=0CCgQFjAB&url=http%3A%2F%2Fwiki.analog…)

Outcomes