AnsweredAssumed Answered

ADV7802 maximum operating temperature range

Question asked by Vidhas on May 18, 2015
Latest reply on Jun 22, 2015 by Vidhas

Hi there,

 

what is the ADV7802 maximum operating temperartue range?

I can see on its data sheet that the Temperature range column indicates "0°C to +85°C”. 

My question is what is its maximum operational range?

This information is not present in the ABSOLUTE MAXIMUM RATINGS of page 10 of the data sheet.


If the ADV7802 maximum minimal operational temperature is 0°C can you suggest a different chip with a lower minimal operational temperature?

I'm looking for a Video decoder that supports 1080p capable of digitizing RGB graphics signals with a maximum operating temperature range of -40°C to +70°C.


Thank you.

Outcomes