AnsweredAssumed Answered

AD9910 USB Firmware

Question asked by Heath on Mar 14, 2011
Latest reply on Mar 16, 2011 by DSB

I have used the AD9910 Evbd extensivly in windows using the supplied software without any problems. I now have to operate the board using Linux. I have had no problems with comunicating with the Cypress USB device using the standard library libusb-1.0. The problem arises when loading the firmware into the USB device. I have looked through the source code of the supplied software and dont see any firmware file.

Am I correct in assuming the device driver dose the loading of the firmware and has it biult in?

Is it possible to get a copy of the firmware so I can just load it using the libusb-1.0 library?

Many thanks

Outcomes