AnsweredAssumed Answered

ZED board set up to run custom made AD9361 FMC cards

Question asked by obalaj Employee on May 15, 2015
Latest reply on May 21, 2015 by mhennerich

Hi,

 

Our client is trying to use the ZED board and the software package (Linux based) to drive his own AD9361 board.

What we learned from this exercise is that the Gui won’t start with AD9361 control tabs if only SPI between AD9361 circuit and the Zed board is established. Can you please let us know which are the hardware conditions we need to present at the FMC connector in order to have a correct boot up of the GUI ?

 

 

Thanks

Ovidiu.

 

 

Outcomes