AnsweredAssumed Answered

Potential JTAG lock-out on ADuC7024 if P0.3 configured as ADC_BUSY?

Question asked by ADUzer on Mar 7, 2011
Latest reply on Mar 9, 2011 by ADUzer

Hello.

 

If P0.3 on the ADuC7024 is configured to have the ADC_BUSY function could this cause JTAG access to be locked out, as that pin's function is also JTAG TRST?

 

Since doing this I get the following message from a programmer "TCK(pin 9) low, but should be high. Please check target hardware.".

 

If locked out because of this, I assume the only way to recover is to perform a mass-erase with ARMWSD.

 

Thanks.

Outcomes