AnsweredAssumed Answered

AD598 single supply range

Question asked by _Robert_ on May 14, 2015
Latest reply on Jun 25, 2015 by harryh

Hi,

 

I have a question concerning the single supply range for the AD598.

In the datasheet it says the operating range is 13 to 36V.

2 lines below, its stated more specifically, that the input voltage must exceed 17,5V to be able to generate a 0 to 10V output.

In my application I have a remote device with >13.5V from the battery and would be satisfied with an AC output range of only +/-2V, not considering the DC offset of the output.

 

Will the AD598 be able to manage that?

If not, what is the minimal voltage for an output range as mentioned above?

Thanks in advance!

 

Cheers Robert

Outcomes