AnsweredAssumed Answered

Limiter Values

Question asked by db10 on Mar 3, 2011
Latest reply on Jun 6, 2013 by JJoseph

Sigma Studo Help does not explicitly define the valid range of values for the Limiter Threshold Parameter (the example graph shows a curve that only reaches 0dB).

 

-What is the valid range of values?

 

-What is the resolution?

 

-If the valid range extends to +24dB does the limiter function as a limiter over the entire range? (e.g. some compressors stop compressing when the input is greater than 6dB).

Outcomes