AnsweredAssumed Answered

Creating Loader file for 21469 with code in External 16 bit DDR2 Memory

Question asked by stevet1976 on Mar 2, 2011
Latest reply on Apr 22, 2011 by DivyaS

I'm trying to  create a loader file for a project which needs to run code from external DDR2 16 bit wide memory.

 

The project is built to generate VISA code.

 

The kernel loads the program OK until it reaches a segment with a data tag of 0x0A (INIT_EXT16). Here the count of the words in the segment seems to be calculated incorrectly.

 

The loader options are set to build with Boot Type = Parallel Port, Format=Ascii, Width=32.

Outcomes