AnsweredAssumed Answered

ADV7611 output port

Question asked by HankZ on Feb 25, 2011
Latest reply on Mar 27, 2012 by Elle

I would like to find out what the capabilities are of the digital output port of the ADV7611.

1) When you select BT-656 output mode up to what frequency will the pixel output clock go.

2) Does it support BT-1120 output mode. I notice that it does support 16 bit BT-656 which should be close but I am not sure if it is the same.

The chip I will hook up to can support BT-656 input up to 120MHz and BT1120 up to 74MHz.  This is OK in that they are willing to drop higher resolutions like 1080p/60 and go with 1080p/30.

 

Thanks

Outcomes