AnsweredAssumed Answered

AD5930/32 Suitability

Question asked by daveb1 on Feb 22, 2011
Latest reply on Mar 9, 2011 by LiamR

Hi,

 

I have a requirement to produce a sinewave which is nominally 1MHz but that can be digitally changed in 1kHz steps up to +/-50kHz. It has to be stable to +/-100Hz between 50 & 125 degC. The digital update rate is << 1Hz.

 

Would the AD5930 or AD5932 device be suitable for this requirement? (I can't tell from the datasheets what units the delta_f register refers to)

 

Thanks

Dave

Outcomes