AnsweredAssumed Answered

ADV8005 OSD Initialize Problem

Question asked by zengya on May 12, 2015
Latest reply on May 15, 2015 by zengya

Hi,

I did a ADV8005 board,code runs as follows

 

********************************************************************

  ADI VSP AVR Application Ver V1.81.1

  PLATFORM: EVAL-ADV8005EBZ Rev 0x0

  HDMI-RX:  ADV7625 Rev 0x4082

  HDMI-TX:  ADV8005 Rev 0x6083 without Rovi

  Created:  May 13 2015 At 09:28:49

********************************************************************

 

In MCU SPI read/write ADV8005 register out of the question, the SPI ADV8005 register that information? Or in a Blimp ?

 

**********************************************************************************

ADIAPI_OSDEgInitHardware: Initializing OSD Engine

 

DMA_selfTest: SPI register access failed 100 in 100 times. OSD engine will stop

 

 

FATAL ERROR: removed OSD feature to avoid further errors.

-OSD 07:584 --------    OSD Hardware init failed    --------

**********************************************************************************

Outcomes