AnsweredAssumed Answered

Is external SDRAM required for using USB functionality in BF52x?

Question asked by Shafi on Feb 11, 2011
Latest reply on Feb 14, 2011 by CraigG

Hi

 

  I am using the USB functionality of BF526. I have modified the code that was shipped with Visual DSP5.0  which uses the APIs and was able to successfully create a usb driver(with Analog Devices Support). Will the on chip memory(132 KB) be sufficient if we are using those USB Libraries?

Should i optimise these libraries inorder that i can make it fit into the on chip memory. Do you have the optimised libraries?

 

Thanks and Regards

Shafi

Outcomes