AnsweredAssumed Answered

Queries about ADF7242 with DSSS-OQPSK Modulation

Question asked by adi_yu Employee on Feb 9, 2011
Latest reply on Apr 2, 2012 by fuaiguo

Hi, there

 

I am Alex from China Applications Support Team. Our responsibility is technical supporting the customers in Asia. Here are some queries about ADF7242.

In the datasheet, it is said that the ADF7242 complies with the IEEE 802.15.4-2006 2.4 GHz PHY requirements with a fixed data rate of 250 kbps and DSSS-OQPSK modulation. And it shows that there are modules for DSSS MOD/DEMOD in Figure 2 of Page 5 in the datasheet.

The query is whether ADF7242 could be used for DSSS modulation or OQPSK modulation. A customer from India wants to use it as DSSS transceiver, could ADF7242 afford it?

Thanks in advanced for your help and support! Looking forward to your kind reply!

 

BR,

Alex

Outcomes