AnsweredAssumed Answered

Audio signal transmit through CAN

Question asked by Lemne on Feb 2, 2011
Latest reply on Mar 17, 2011 by gvasanth

Hello ! I have to transmit an audio signal from a blackfin 537 to another blackfin 537. I was thinking that i could do this using two talkthrough's (on each bf537) but i have to do it through CAN. The ideea is that the audio signal is sent using talkthrough to the bf537 no1 and then it must be redirected to the CAN port and then sent to the bf537 no 2 using the mailboxes and over there i have to connect some headsets to the line out and listen to the audio. Any help please ? I tried altering the CAN Tx, CAN Rx and talkthhrough examples but with no use. Thank you ! (using vdsp++ 6) Any code examples of sending signals through CAN ?

Outcomes