AnsweredAssumed Answered

Uart3 Tx frequency measurement

Question asked by jacob on Jan 24, 2011
Latest reply on Jan 30, 2011 by jacob

Hi,

A am using the BF548 Ez kit Eval Board.

Have defined these pll divisors:

(25MHz  x (MSEL=24))  VCO=600MHz        

(600MHz x (SSEL=5))   SCLK=120MHz      

 

my Uart divisor is: 0x0096   ( = 150)  for EDBO = 1. => UART freq should be 800KHz.

 

120MHz/150 = 800KHz

 

 

But, when i am measuring the UART3 TX pin, i see 400 MHz.

 

didn't see anywere that the UART3 gets half of the SCLK freq (as timers get) or any other indication, to expect this to happen

 

How can i solve this problem?

 

Thank!

Jacob

Outcomes